FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > [EcoMonitorPlus] Caution when you are using Basic Unit (Model: EMU4-BM1-MB, EMU4-HM1-MB, or EMU4-LG1-MB) manufactured in October 2016 or before
FAQ
[EcoMonitorPlus] Caution when you are using Basic Unit (Model: EMU4-BM1-MB, EMU4-HM1-MB, or EMU4-LG1-MB) manufactured in October 2016 or before
What is the caution that must be followed when we are using Basic Unit (Model: EMU4-BM1-MB, EMU4-HM1-MB, or EMU4-LG1-MB) manufactured in October 2016 or before?
Answer
Basic Unit manufactured in October 2016 or before is version A, which has restrictions on usage. The connectable number of extension units is two, not three when the following two conditions are met.
■When CC-Link Communication Unit (Model: EMU4-CM-C) of optional units is connected
■When one or more of either Pulse Input Unit (Model: EMU4-PX4) or Analog Input Unit (Model: EMU4-AX4) is added
*Basic Unit (Model: EMU4-BM1-MB, EMU4-HM1-MB, or EMU4-LG1-MB) manufactured in November 2016 or after is all version B, where three extension units can be connected without any conditions.
■When CC-Link Communication Unit (Model: EMU4-CM-C) of optional units is connected
■When one or more of either Pulse Input Unit (Model: EMU4-PX4) or Analog Input Unit (Model: EMU4-AX4) is added
*Basic Unit (Model: EMU4-BM1-MB, EMU4-HM1-MB, or EMU4-LG1-MB) manufactured in November 2016 or after is all version B, where three extension units can be connected without any conditions.
To check the product version, refer to the following illustration.
- Product Name
- Energy Measuring Unit
- Series
- EcoMonitorPlus
May I have your opinion?
Related FAQ
- Sample program for CC-LINK communication (EcoMonitorPlus/EcoMonitorLight)
- [EcoMonitorPlus] Caution when you are using Display Unit (Model: EMU4-D65) manufactured in October 2016 or before
- Active energy (lower digit indication) display upon communication test of MODBUS RTU/TCP communication (ME96SS series).
- As to required number of Display Unit.
- Replied value on the communication operation test of test mode (ME96SS series).