FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Network/Communication > Regarding error 2440H on CPU module when using FX5-CCLGN-MS
FAQ
Regarding error 2440H on CPU module when using FX5-CCLGN-MS
If the communication interval setting value is not set to a sufficient length on FX5-CCLGN-MS, error 3013H occurs. Why does this cause error 2440H on the CPU module?
Answer
When the power is turned on, the FX5-CCLGN-MS performs parameter check processing, and if an error occurs, the CPU module is also notified of the error. Therefore, an error code is also generated on the CPU module side. Resolving the FX5-CCLGN-MS error also clears the CPU module error.
- Product Name
- FX5-CCLGN-MS
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series