Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 39314
  • Release Date : 2023/01/12 16:54
  • Print

Regarding number of input/output points when adding safety extension module

If the FX5-SF-MU4T5 is added, will the number of I/O points that can be added to the FX5 CPU module be affected?
Category : 

Answer

It will. It is treated the same as an intelligent module, so it occupies 8 I/O points. The safety input expansion module FX5-SF-8DI4 does not occupy the number of I/O points even when it is expanded.
Product Name
FX5-SF-MU4T5、FX5-SF-8DI4
Product Category
CPU Module, Safety Control
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries