FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding input of Differential Driver Output Type
FAQ
Regarding input of Differential Driver Output Type
Does the FX5 CPU module's built-in high-speed counter function allow pulse input from a DC5V differential driver output type encoder?
Answer
It does not. The built-in high-speed counter function of the FX5U/FX5UC CPU module does not support DC5V input.
DC5V input can be achieved by adding BUS conversion module FX5-CNV-BUS(C) + FX5-2HC/ES.
*The FX5-2HC/ES can be added to the FX5U/FX5UC/FX5UJ CPU modules.
- Product Name
- FX5U,FX5UC,FX5UJ,FX5S,FX5-2HC/ES
- Product Category
- CPU Module, High-Speed Counter
- Series
- MELSEC iQ-F Series