FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding maximum number of connections for the simple CPU communication function
FAQ
Regarding maximum number of connections for the simple CPU communication function
What is the maximum number of connections for the simple CPU communication function of the FX5 CPU module?
Answer
The maximum number of connections for the simple CPU communication function of FX5 CPU module is 16 for FX5U/FX5UC CPU module and 8 for FX5UJ/FX5S CPU module. In addition, by adding FX5-ENET and FX5-ENET/IP to FX5U/FX5UC/FX5UJ CPU module , it is possible to connect an additional 32 modules.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S, FX5-ENET, FX5-ENET/IP
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series