FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Analog > Regarding Control response parameter of built-in PID Control of CPU Module
FAQ
Regarding Control response parameter of built-in PID Control of CPU Module
What is the difference between "normal" and "fast" control response parameter of built-in PID control of CPU Module?
Answer
The control response parameter can set the response to the target value (SV) of PID control as either "normal" or "fast". The difference is as follows.
(1)When "Normal" is set, the time to reach the target value (SV) will be longer, but overshoot/undershoot will be suppressed.
(2)When set to "Fast", the time to reach the target value (SV) will be shorter, but the overshoot/undershoot will be larger.
For details, refer to the following manual.
MELSEC iQ-F FX5 User's Manual (Application)
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module,Analog
- Series
- MELSEC iQ-F Series