FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Automation Controllers MELSEC > MELSEC MX Controller MX-F Model > Regarding built-in ethernet port differences
FAQ
Regarding built-in ethernet port differences
The MX-F model has 2 built-in Ethernet ports. Is there any difference?
Answer
Port 1 becomes the CC-Link IE TSN, and port 2 can be switched between Ethernet and CC-Link IE TSN.
To use port 2 as an Ethernet port, set the Built-in Network Type to "Ethernet + CC-Link IE TSN" when creating a new project in GX Works3.
To use port 2 as the CC-Link IE TSN port, set the Built-in Network Type to "CC-Link IE TSN" when creating a new project in GX Works3.
To switch Port 2 while creating a project, select [Project] ⇒ [Change Module Type/Operation Mode] in GX Works3 and select [Built-in Network Type].
- Product Name
- MX-F Model
- Series
- MELSEC MX Controller