Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 44980
  • Release Date : 2025/05/08 09:08
  • Print

Regarding built-in high-speed counter function

The CPU Module of the iQ-F series supports the built-in high-speed counter function, but does the MX-F Model also support it?

Category : 

Answer

The MX-F Model also supports the built-in high-speed counter function.

The number of channels is up to 8, and the counter types supported are 1-phase 1-input/1-phase 2-input/2-phase 2-input (1x/2x/4x)/internal clock (1MHz (fixed)). 

The maximum frequency varies depending on the counter type, but up to 200kHz is supported.

Product Name
MX-F Model
Series
MELSEC MX Controller

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries