FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > Controlling the GOT buzzer
FAQ
Controlling the GOT buzzer
Can the GOT buzzer be sounded intentionally?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
The GOT buzzer can be sounded intentionally.
Set the system information in the screen design software.
The buzzer can be output using the system information (read device).
• Buzzer Three-shot Output signal (System signal 1-1.b8)
• Buzzer Output signal (System signal 1-1.b14)
• Buzzer One-shot Output signal (System signal l 1-1.b15)
◆ For GT Designer3 (GOT2000) Version 1
1. Set the system information read device.
Select [Common] - [GOT Environmental Setting] - [System Information], and then select [Use System Information].
Set a device for [System Signal 1-1].
2. Turn on b8, b14, or b15 of System signal 1-1 using the GOT or sequence program.
The buzzer is output.
* The buzzer volume cannot be changed.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (buzzer output)
- Series
- GOT2000 Series, GOT3000 Series