FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT15 > How to control GOT buzzer from the PLC
FAQ
How to control GOT buzzer from the PLC
Can the GOT buzzer be controlled from the PLC?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT15
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT16
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT11
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT10
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT14
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software > HMI/GOT Screen Design Software
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT1000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
The GOT buzzer can be controlled from the PLC.
Use the system information (read device).
• Buzzer Three-shot Output signal (System signal 1-1.b8)
• Buzzer Output signal (System signal 1-1.b14)
• Buzzer One-shot Output signal (System signal 1-1.b15)
Set the system information using the screen design software.
(Example) Control the buzzer sound by using D0 for System signal 1-1.
◆ GT Designer3 (GOT2000) Version 1
1. Select [Common] → [GOT Environmental Setting] → [System Information] to open the [Environmental Setting] setting dialog.
2. Select [Use System Information] and configure each setting.
• [First Device] for [Read Device (Controller → GOT)]: D0
• [First Device] for [Write Device (GOT → Controller)]: Any device
After setting the above, turn on b8, b14, or b15 for System signal 1-1 from the PLC.
The buzzer is output.
* The buzzer volume cannot be changed.
The following is an example of a ladder program.
Turn on or off D0.b8, D0.b14, and D0.b15 according to the values of M0, M1, and M2.
Figure 1

- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (standard function), GT SoftGOT2000, GT SoftGOT1000, GT SoftGOT3000
- Series
- GOT2000 Series, GOT1000 Series, GOT Screen Design Software, SoftGOT2000, GOT3000 Series, SoftGOT3000