FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25 > How to control the screen saver from the PLC
FAQ
How to control the screen saver from the PLC
Can I control the screen saver from the PLC?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
The screen save can be controlled from the PLC.
Use the system information (read device).
When the Forced Screen Saver Enable signal (System signal 1-1.b1) is turned on and off, the screen saver can be controlled.
Set the system information using the screen design software.
(Example) Control the screen saver by using D0 for System signal 1-1.
The following is an example of a ladder program.
(Example 1) Turn on or off D0.b1 according to the value of M0.
Figure 1

(Example 2) Turn on D0.b1 at the rising edge of M0 and turn off D0.b1 at the falling edge of M0.
Figure 2

◆ For GT Designer3 (GOT2000) Version 1
1. Select [Common] → [GOT Environmental Setting] → [System Information] to open the [Environmental Setting] dialog.
2. Select [Use System Information] and configure each setting.
Figure 3

- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (standard function), GT SoftGOT2000, GT SoftGOT3000
- Series
- GOT2000 Series, SoftGOT2000, GOT3000 Series, SoftGOT3000