FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25 > When a negative value is displayed on the numerical display instead of a positive value
FAQ
When a negative value is displayed on the numerical display instead of a positive value
The value should be 40000, but a negative value is displayed when the device value is monitored with the numerical display.
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
If a negative value is displayed instead of 40000 when monitoring the device value on the numerical display, check the numerical display settings in the screen design software.
(Example) If the device value in the Mitsubishi Electric PLC data register (D0) should be 40000 but a negative value is displayed, monitor the device value with an unsigned word.
◆ For GT Designer3 (GOT2000) Version 1
Configure the following settings:
Figure 1

The data range differs depending on the setting for the PLC data type.
Check the data range.
Then check the settings for data type and display type.
Use the combination of data type and display type in Figure 2.
Figure 2

For (C) and (D) in Figure 2, the two devices are used to display the values.
• For D0=1234(H) and D1=5678(H), when D0 is monitored with a numerical display, it shows 56781234(H) (1450709556 in decimal).
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (numerical display/text display), GOT function (numerical input/text input), GT Designer3
- Series
- GOT2000 Series, GOT Screen Design Software, SoftGOT2000, GOT3000 Series, SoftGOT3000