FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > An object used to change the displayed character string according to the device value
FAQ
An object used to change the displayed character string according to the device value
What objects are available to switch the displayed character string by turning the bit device on or off?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
The following objects are available to switch the displayed character string by turning the bit device on or off.
1. Bit comment
Use this object to display the fixed character string (ON or OFF) or switch between ON and OFF by turning the bit on or off.
2. Word comment
Use this object when there are multiple display patterns of fixed character strings.
3. Text display
Use this object to display character strings (variable character strings/character code expressions) stored in the word device.
◆ For GT Designer3 (GOT2000) Version 1
Figure 1 shows the locations where the above-mentioned objects can be selected in GT Designer3 (GOT2000).
Figure 1

When using a bit comment or word comment, set the bit comment (Fig. 2) or word comment (Fig.3).
Figure 2

Figure 3

To display a fixed character string, use a bit comment or word comment.
The text display interprets the data stored in the word device as character codes (ASCII code, Unicode, Shift JIS code, GB code, KS code, or Big5 code) and displays the text.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (numerical display/text display), GOT function (numerical input/text input), GOT function (comment display)
- Series
- GOT2000 Series, GOT Screen Design Software, SoftGOT2000, GOT3000 Series, SoftGOT3000