FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > How to set the network number and station number for connection to RCPU and QnUD(P)VCPU
FAQ
How to set the network number and station number for connection to RCPU and QnUD(P)VCPU
How do I connect the RCPU or QnUD(P)VCPU to the GOT by setting the network number and station number using project data transfer via the PLC or other methods?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
To connect the RCPU or QnUD(P)VCPU to the GOT by setting the network number and station number using project data transfer via the PLC or other methods, configure the MELSOFT connection extension settings with the engineering tool of the controller.
When using the MELSOFT connection extension settings, match the network number and station number of the RCPU or QnUD(P)VCPU with those of the screen design software.
The port number is 5001.
1. RCPU
Use the RCPU firmware version specified in the following reference:
MELSEC iQ-R Ethernet User's Manual (Application) (SH-081257ENG)
"Communications by network number/station number" in "Appendix Added and Enhanced Functions"
To look up the RCPU firmware version, refer to the following:
MELSEC iQ-R Module Configuration Manual (SH-081262ENG)
"Appendix 1 Checking Production Information and Firmware Version"
◆ For GX Works3 Version 1.050C or later
Go to the navigation window then select → [Parameter] → [RnCPU] → [Module parameter] → [Basic Settings] → [Own Node Settings]
→ [Communications by Network No./Station No.]
Figure 1

◆ For GT Designer3 (GOT2000) Version 1
[Common] → [Controller Setting]
Figure 2

2. QnUD(P)VCPU
Use a QnUD(P)VCPU with a serial number that contains the number "17052" or higher in the first 5 digits.
◆ GX Works2 Version 1.535H or later
Navigation window → [PLC parameter] → [Built-in Ethernet Port Setting] → [MELSOFT Connection Extended Setting]
Figure 3

◆ For GT Designer3 (GOT2000) Version 1
[Common] → [Controller Setting]
Figure 4

For details on the MELSOFT connection extension settings, refer to the following:
QnUCPU User's Manual (Communication via Built-in Ethernet Port) (SH-080811ENG)
"3.5 MELSOFT Connection Extended Setting"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (communication)
- Series
- GOT2000 Series, GOT3000 Series