FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25 > Touch switch not displayed on the GOT
FAQ
Touch switch not displayed on the GOT
The touch switch is not displayed on the GOT.
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software > HMI/GOT Screen Design Software
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
If the touch switch is not displayed on the GOT, check the switch setting in the screen creation software.
◆ For GT Designer3 (GOT3000) Version 1
If the following settings are configured, the touch switch will not be displayed on the GOT.
1. In the [Basic Settings] tab, if [Lamp (Timing to change shape/text)] is set to [Bit-ON/OFF] or [Word Range], a device outside of the specified device range is set in the controller.
2. In the [Basic Settings] tab, [Shape] in [Style] is set to "None".
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (alarm)
- Series
- GOT2000 Series, GOT3000 Series, SoftGOT2000, SoftGOT3000, GOT Screen Design Software