FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27 > Checking the screen number of the displayed screen on the GOT
FAQ
Checking the screen number of the displayed screen on the GOT
Can the screen number displayed on the GOT be monitored with the PLC?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT15
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT16
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT11
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT10
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT14
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software > HMI/GOT Screen Design Software
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT1000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
The screen number displayed on the GOT can be monitored with the PLC. Perform one of the following operations.
1. Monitor the screen switching device.
Set the PLC device for the screen switching device to monitor the device.
2. Monitor system information.
Set the PLC device for [System Signal 2-1] in System Information, and select the following items to monitor the device.
• [On-screen Window Base Screen Number]: Base screen number
• [On-screen Window1 Screen Number]: Overlap window 1 screen number
• [On-screen Window2 Screen Number]: Overlap window 2 screen number
• [On-screen Window3 Screen Number]: Overlap window 3 screen number
• [On-screen Window4 Screen Number]: Overlap window 4 screen number
• [On-screen Window5 Screen Number]: Overlap window 5 screen number
GT21, GT15, GT14, GT11, and GT10 are only compatible with window screens 1 and 2.
For details, refer to the screen design software manual.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (standard function)
- Series
- GOT1000 Series, GOT2000 Series, GOT3000 Series, GOT Screen Design Software, SoftGOT2000, SoftGOT3000