FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT14 > Converting a logging file (binary format) to a CSV file
FAQ
Converting a logging file (binary format) to a CSV file
How do I convert binary format logging files to CSV format?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT15
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT16
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT11
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT10
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT14
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT1000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
The following methods can be used to convert binary format logging files (*.G3L, *.G2L, or *.G1L) to CSV format.
1. Conversion using the GOT utility function
Example: For the GOT3000 series
Select [Main menu] → [Data mng.] → [Logging information].
2. Conversion using the logging file conversion function of the screen design software
Example: For GT Designer3 (GOT3000) Version 1
Select [Tools] → [Resource Data Conversion] → [Logging File].
3. Automatic conversion when the logging file is created by configuring the additional file output setting in the logging settings of the screen design software
Example: For GT Designer3 (GOT3000) Version 1
Select [Output additional file] in the logging settings dialog then click [Destination].
4. Conversion using the Data Transfer Tool
There are multiple conversion methods using the Data Transfer Tool.
• Select [Menu] → [Resource Data Conversion].
• Convert resource data from the command line.
• Convert resource data using the interface functions.
For details, refer to the manuals of the screen creation software and the Data Transfer Tool.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (logging)
- Series
- GOT3000 Series, GOT2000 Series, GOT1000 Series, SoftGOT3000, SoftGOT2000, SoftGOT1000