FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT15 > How to display integer values written to the PLC as real numbers (with decimal points) on the GOT
FAQ
How to display integer values written to the PLC as real numbers (with decimal points) on the GOT
How do I display integer values written to the PLC as real numbers (with decimal points) on the GOT?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT15
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT16
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT11
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT10
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT1000 Series > GT14
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software > HMI/GOT Screen Design Software
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT1000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
Use the automatic decimal place adjustment function to display the integer value written to the PLC as a real number on the numerical display on the GOT.
Configure the settings in the screen design software.
◆ For GT Designer3 (GOT2000) Version 1
Configure the following settings.

If the value 123 is written to the specified device (D0), 1.23 is displayed on the numerical input object.
To display the device value 123 as 123.00, deselect the automatic decimal place adjustment function.
For details, refer to the screen design software manual.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (numerical input/text input)
- Series
- GOT1000 Series, GOT2000 Series, GOT3000 Series, GOT Screen Design Software, SoftGOT2000, SoftGOT3000