• No : 20837
  • Release Date : 2018/08/22 16:24
  • Print

Safety stop function of the FR-D700/FR-E700

Can the category 3 be satisfied even when the magnetic contactor, which is described as the safety stop function connection example in the Instruction Manual, is not installed on the input side of the inverter?
Category : 

Answer

It is recommended to install the magnetic contactor on the input side of the inverter for safety. The category 3 can be satisfied without installing it.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-D700, FR-E700