• No : 20920
  • Release Date : 2018/08/22 16:25
  • Print

FR-A8NC

When the torque limit is input via the CC-Link, what happens if a negative value is written to the torque limit? For example, what happens when -100% is written?
Category : 

Answer

The torque limit setting is defined as an absolute value. Thus, when -100% is written to the torque limit, the torque is limited at 100%.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
Option