• No : 20979
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800

What is the "maximum output frequency" of the frequency accuracy in the common specification: "Within ± 0.2% of the maximum output frequency"?
Category : 

Answer

It is based on the maximum value that can be set for frequency. Specifically, it is 400 Hz.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800