• No : 21593
  • Release Date : 2018/08/22 16:28
  • Print

What are the specifications of totally enclosed type?

What are the specifications of the totally enclosed type?
Category : 

Answer

The totally enclosed type is JEM1030 IP40.
(IP40: Structure that prevents the tip of a solid object exceeding 1 mm in diameter or thickness (wire or steel belt) from entering the inside)Be sure to use it in the surrounding air temperature of -10 to + 40 deg C.
Product Name
Inverter, magnet motor drive
Product Category
Common
Series
FR-U100