- No : 21702
- Release Date : 2018/08/22 16:29
-
Print
FR-PA07
I am using the optional operation panel FR-PA07 connected with a cable with Pr.79 (Operation mode) set to "3".
How can I switch between the setting dial and multi-speed settings?
- Category :
-
Answer
There is a priority between the setting dial and multi-speed settings.
Since the multi-speed setting is given a higher priority, the setting by the setting dial does not take effect unless all of the multi-speed signals are OFF.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ