- No : 21730
- Release Date : 2018/08/22 16:29
-
Print
Operation panel (FR-PA02)
Can I keep using the operation panel FR-PA02 that is used with the FR-E500?
How should I set the inverter to do this?
- Category :
-
Answer
Set Pr.146 (Built-in potentiometer switching) to "0".
This allows for using the potentiometer built in the FR-PA02 to set the frequency.
(Set this parameter to "1" when the built-in potentiometer is not used.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ