- No : 22720
- Release Date : 2018/09/03 17:29
-
Print
Pulse width with which the QX42 recognizes all pulses
How wide is the pulse width with which the QX42 recognizes all pulses with the set response time? For example, when 10 ms has been set as the response time with the scan time of 10 ms, how wide is the pulse width with which the module recognizes all input pulses?
- Category :
-
Answer
Maximum scan time (10 ms) + Response time (10 ms) = Pulse width with which the module recognizes all pulses (20 ms)
- Product Name
- MELSEC-Q Series
- Series
- Input Module