• No : 22721
  • Release Date : 2018/09/03 17:29
  • Print

Hardware setting for using Q series extension base units

Do I need to configure any hardware setting to use Q series extension base units?
Category : 

Answer

You need to set the number of extension base units with the connector for setting the number of extension base units.
For details, refer to the following.
SH-080473 QCPU User's Manual (Hardware Design, Maintenance and Inspection)
4.3 Connecting an Extension Base Unit
Product Name
MELSEC-Q Series
Series
CPU