- No : 22784
- Release Date : 2018/09/03 17:30
-
Print
SD1284 of LCPU with built-in Ethernet port
During socket communication of L series CPU with built-in Ethernet port, how does the special register SD1284 (Open request signal) correspond to the connection number?
- Category :
-
Answer
The bits 0 to F of the special register SD1284 (Open request signal) correspond to the connection numbers 1 to 16. When the open request is sent, the corresponding bit will turn ON.
- Product Name
- MELSEC-L Series
- Series
- L Series