- No : 23012
- Release Date : 2018/09/03 17:31
-
Print
Connecting the CC-Link IE Field Network with a personal computer
Can I use a commercial personal computer as one of CC-Link IE Field Network stations if the computer has the 1000BASE-T port on it and the port is directly connected?
- Category :
-
Answer
To pursue high speeds, the CC-Link IE Field Network applies a communication control method different from that applied to the Ethernet communication for personal computers. Hence a personal computer cannot be directly connected to the CC-Link IE Field Network. Connect the computer to the Network via the Ethernet adapter module NZ2GF-ETB.
- Product Name
- Network Related Products
- Series
- CC-Link IE Field Network