• No : 23079
  • Release Date : 2018/09/03 17:31
  • Print

Cause to turn on the ERR LED of a CC-Link master module

What makes the ERR LED of a CC-Link master module turn on?
Category : 

Answer

All stations communication error of a slave station.

When POWER of the slave station is off, check if 24 V DC has been supplied.

When POWER is on, check the station number and transmission speed setting of the slave station and check the cable for a disconnection or improper wiring.
Product Name
Network Related Products
Series
CC-Link