• No : 23178
  • Release Date : 2018/09/07 16:09
  • Print

Brake is not working properly.

Answer

Cause:

[Occurs only when operating manually]
•T/B operation error.
[Occurs when operating manually and automatically]
•Faulty connection of the cables that run between devices.
•Brake failure.

Measures:

[Occurs only when operating manually]
•Check the T/B operation(operation buttons, 3 position enabling switch, etc.).
[Occurs when operating manually and automatically]
•Check the mating of the cables that run between devices.

Product Name
Industrial Robots MELFA
Series
FR Series