FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
Port number when using the Ethernet connection
Back
No : 23451
Release Date : 2018/09/14 15:06
Update : 2018/09/26 18:45
Print
Port number when using the Ethernet connection
When multiple GOT2000 series models are connected to one PLC by Ethernet, is the GOT communication port number required to be changed?
Category :
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
GT27
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
GT25
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
GT21
Answer
When multiple GT27, GT25, or GT21 models (Ethernet connection models) are connected to one PLC by Ethernet, the GOT communication port number is not required to be changed.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication)
Series
GOT2000 Series