• No : 23507
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 17:26
  • Print

Specifications of the white model

What is the difference between the white model and standard model of GT27and GT25 in addition to the color?
Category : 

Answer

Differences between the white model and standard model of GT27 and GT25 are as follows.
 ・ The front face is white-colored.
 ・ The USB interface is located on the back, and the front face is flat-shaped.
 ・ The GOT complies with the safety standards (ATEX Directive (*1), KCs Regulation (*1), and UL Class I Division 2).
 ・ The number and locations of USB hosts (white model: one channel (back), standard model: two channels (front and back))
 ・ The location of the USB device (white model: one channel (back), standard model: one channel (front))

(*1) The ATEX Directive and KCs Regulation apply only to DC models.
  The models that apply to the ATEX Directive or KCs regulation require an optional protective sheet (GT25-□□PSCC-UC) and special fittings (GT25-□□FIT-EXS).
(GT2508-VTWD requires a protective sheet only.)
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT
Series
GOT2000 Series