- No : 23522
 
      - Release Date : 2018/09/14 15:07
 
        - 
          
              Print
          
        
 
  
 
Using the rugged model outdoors
    
      Can the rugged model be used outdoors?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    The rugged model can be used outdoors. 
Protect the GOT from direct sunlight by attaching a roof or in other ways when using the rugged model outdoors. 
Due to direct sunlight, the temperature of the panel surface and inside the control panel may increase. Use the GOT in the environment within the operating ambient temperature range.
  
    
      
        - Product Name
 
          - Human-Machine Interfaces(HMIs)-GOT
 
      
      
        - Product Category
 
          - Rugged model
 
      
      
        - Series
 
          - GOT2000 Series