• No : 23529
  • Release Date : 2018/09/14 15:07
  • Update : 2018/09/25 17:19
  • Print

Cleaning the rugged model with its power on

Answer

The GOT cannot be cleaned with its power on.

Turn off the power before cleaning the GOT. Check the following before cleaning.
・ The GOT is mounted to the control panel correctly.
・ The environmental protection sheet (not replaceable) is in the normal condition.

If the environmental protection sheet peels or the cleaning solution enters between the environmental protection sheet and the display section during cleaning, stop the cleaning immediately. Do not use the GOT in this condition.

This applies to the rugged model as well.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model
Series
GOT2000 Series