• No : 23531
  • Release Date : 2018/09/14 15:07
  • Update : 2018/09/25 17:18
  • Print

Setting a password to the rugged model

Answer

A password can be set to the rugged model.
A password can be set to the GOT individually for each case when the security is required.

・ Setting a password to change the contents of the screen display for each user
   → Level authentication or operator authentication
・ Setting a password to restrict invalid data reading and writing
   → Data transfer security
・ Setting a password to restrict the utility startup and password setting screen display
   → Functional operation security

For the details, refer to the following.
GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG-W)
"5.2.8 Configuring the security settings for displaying screen data on the GOT ([Screen Security] (Level authentication))"
"5.2.7 Configuring the security settings for displaying screen data on the GOT ([Screen Security] (Operator authentication))"
"5.2.10 Configuring the security setting for transferring data ([Data Transfer Security])"
"5.2.9 Configuring the security settings for operating the utility and the monitor functions ([Functional Operation Security])"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model, GOT function (screen security), GOT function (functional operation security), GOT function (operator authentication)
Series
GOT2000 Series