• No : 23548
  • Release Date : 2018/09/14 15:07
  • Print

Surface treatment of the front face of the rugged model

Answer

The surface treatment of the front face of the rugged model is the AG (antiglare) treatment for both the environmental protection sheet and optional UV protective sheet.
The environmental protection sheet and optional UV protective sheet are made from UV cutoff materials. (95% UV cutoff with a sheet of 370nm)
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model, GOT function (UV protective sheet)
Series
GOT2000 Series