• No : 23705
  • Release Date : 2018/09/19 17:16
  • Print

The viewpoint of the definite time factor characteristic graph

What do the figures on the horizontal axis of the definite time factor characteristic graph mean?
Category : 

Answer

It means multiples of the settling value. For example, when a definite time factor operation settling value of a relay is 3 A, 1x is read as 3 A and 5x is read as 15 A.
Product Name
Protection Relay
Series
MELPRO-A Series