• No : 25233
  • Release Date : 2019/09/02 16:01
  • Print

Regarding automatically restart of Windows

Is it possible to build a system that automatically restarts Windows when Windows does not start (WIN RDY LED flashes)?
Category : 

Answer

It is possible to build a system to restart Windows automatically by VxWorks user program.
The implementation example is described below.
[Windows start monitoring system]
・ Monitor that the status of "WIN RDY LED" changes from "flashing" to "lighting" with the "CCPU_GetLEDStatus" function.
・ If the status of "WIN RDY LED" does not change to "ON" for a certain period,
    the "CCPU_WinReset" function forces the Windows part to restart.
Product Name
MELIPC
Series
MI5000