• No : 20820
  • Release Date : 2018/08/22 16:24
  • Print

Combination of the FR-F800 and MM-EFS

Can the MM-EFS of one-rank lower capacity be used with the FR-F800?
Category : 

Answer

Yes, it can. Set "12" or "112" to the MM-EFS capacity used for Pr.80 (Motor capacity) and Pr.998 (PM parameter initialization).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-F800