- No : 20869
- Release Date : 2018/08/22 16:24
-
Print
FR-E700KNC
Is the inverter reset when the power supply +24 is turned ON and OFF to reflect the parameter such as Pr.542 on the condition that on only +24 is input from the external input terminal?
- Category :
-
Answer
The inverter is reset.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700