- No : 20873
- Release Date : 2018/08/22 16:24
-
Print
FR-A8NC
I read the status such as alarms via the CC-Link when the main circuit is OFF and the control circuit is ON. If the main circuit is turned ON on this condition, the inverter reset is not performed but the error signal is turned OFF for one second. What is the reason for this?
- Category :
-
Answer
Because the inverter status reading is stopped by the processing such as PLC in the inverter when the main circuit turns ON. It is stopped for approximately one second.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option