- No : 20874
- Release Date : 2018/08/22 16:24
-
Print
FR-A8TP
In New Product RELEASE, it is described that the encoder power supply of both 12 VDC and 24 VDC can be used for the SF-V5RU. Is it also true for the SF-V5R because its encoder is the same as the SF-V5RU one?
- Category :
-
Answer
Yes, it is.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option