- No : 20875
- Release Date : 2018/08/22 16:24
-
Print
FR-A8NC
When supplying the 24 VDC power, why can Pr.542 (station number setting) be read without connecting the FR-A8NC?
- Category :
-
Answer
When the 24 VDC power is supplied, optional parameters can be read.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option