• No : 20876
  • Release Date : 2018/08/22 16:24
  • Print

FR-A8TR

As the restriction of the FR-A8TR, it is described that the terminals +24, 10E, 4, and STOP are unavailable when the FR-A8NC is used. What is the reason for that?
Category : 

Answer

Because when the FR-A8NC and FR-A8TR are used together, the wiring to the terminals becomes physically difficult.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
Option