• No : 20887
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800-R2R

What is the initial winding diameter value when the initial winding diameter calculation is not performed?
Category : 

Answer

When the value is written to Pr.646 (Stored winding diameter), the stored value is used. When the value is not written, the minimum or maximum winding diameter value is used. Which one to be used depends on whether the operation is winding or unwinding. (minimum value at the winding/maximum value at the unwinding)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800-R2R