• No : 20888
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800-R2R

When the winding diameter calculation is the thickness method and the normal speed control is performed, how can I set the initial speed to 20 Hz and the end speed to 40 Hz?
Category : 

Answer

They cannot be set with the frequency. Because the command is input at the line speed, consider the line speed of the initial winding diameter at 20 Hz. The frequency at the winding ending is determined by the result of the winding diameter calculation.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800-R2R