- No : 20890
- Release Date : 2018/08/22 16:24
-
Print
FR-A800-R2R
Can I operate the winding diameter calculation function without a sensor or encoder?
- Category :
-
Answer
The encoder feedback is always required for the thickness calculation function. The actual line speed calculation function requires the input of the actual line speed. For the actual line speed calculation, the encoder feedback is not required.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800-R2R