- No : 20893
- Release Date : 2018/08/22 16:24
-
Print
Load characteristics fault detection
When Pr.1480 (Load characteristics measurement mode) is set to "1" with the load characteristics fault function, the load characteristics load reference is set to Pr.1481 to 1485. Is this load standard value related with Pr.56 (Current monitoring reference)?
- Category :
-
Answer
Only the V/F control is related with Pr.56. The motor torque is calculated from the current value (not Pr.56) and motor constant. For the V/F control, it is calculated from the value of Pr.56.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F800