- No : 20943
- Release Date : 2018/08/22 16:25
-
Print
CC-Link
Is it possible to import all signals of warning and alarm via the CC-Link using FR-A800+FR-A8NC?
- Category :
-
Answer
For output signals, up to 10 points (RXn2 to RXB) can be assigned. It is possible if the number of the importing signal points are within this range.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option