• No : 21020
  • Release Date : 2018/08/22 16:25
  • Print

Built-in braking resistor

Is the resistance value of the internal resistor of the FR-A800 (7.5K or lower) same as that of the FR-A700?
Category : 

Answer

Yes, the resistance values are the same.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800